BLE_DD_Init
C
bool BLE_DD_Init(void);Description
Initializes the BLE Device Discovery (BLE_DD) module.
Return values
| Return value | Description |
|---|---|
| true | Initialization of the BLE_DD module was successful. |
| false | Initialization of the BLE_DD module failed. |
bool BLE_DD_Init(void);Initializes the BLE Device Discovery (BLE_DD) module.
| Return value | Description |
|---|---|
| true | Initialization of the BLE_DD module was successful. |
| false | Initialization of the BLE_DD module failed. |