BLE_SMP_EncInfo_T
C
typedef struct BLE_SMP_EncInfo_T
{
uint8_t ltk[16];
uint8_t ediv[2];
uint8_t randNum[8];
unsigned int lesc:1;
unsigned int auth:1;
unsigned int ltkLen:6;
}BLE_SMP_EncInfo_T;Description
Structure for encryption information used in BLE connections.
Field Documentation
| Field | Description |
|---|---|
| ltk | Long Term Key (LTK). Used to encrypt the connection. |
| ediv | Encrypted Diversifier (EDIV). A value used in the key derivation process. |
| randNum | Random Number (Rand). Used alongside the EDIV to identify the LTK. |
| lesc | LE Secure Connections flag. Indicates if the key was generated using LE Secure Connections. |
| auth | Authenticated Key flag. Indicates if the LTK is an authenticated key. |
| ltkLen | Length of the LTK in bytes. |