BLE_TRSPC_SendVendorCommand
C
uint16_t BLE_TRSPC_SendVendorCommand(uint16_t connHandle, uint8_t commandID, uint8_t commandLength, uint8_t *p_commandPayload);Description
Sends a vendor-specific command over the BLE connection.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Connection handle associated with this connection. |
| [in] commandID | The identifier for the vendor-specific command. |
| [in] commandLength | The length of the command payload. |
| [in] p_commandPayload | Pointer to the command payload data. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | The command was successfully sent. |
| MBA_RES_FAIL | The connection is invalid or the CCCD of TCP is not enabled. |
| MBA_RES_OOM | Internal memory allocation failure. |
| MBA_RES_INVALID_PARA | The commandID or commandLength is invalid. |