Defines
- Address length
Defines the maximum length of a Bluetooth address.
- Address types
Defines the different types of BLE device addresses.
- Advertising
channels
Defines the advertising channel indices that can be used for BLE advertising.
- Advertising filter
policies
Defines the policies for filtering advertising packets.
- Advertising
interval
Defines the range for advertising intervals in units of 0.625 ms.
- Advertising
options
Defines the advertising option.
- Advertising Set Identifier
(SID) range
Defines the range of values for the Advertising Set Identifier (SID).
- Advertising
types
Enumerates the different types of advertising that can be performed.
- Appearance
definitions
Defines the standard appearance values used in GAP (Generic Access Profile).
- Operation of extended
advertising data
BLE LIB supports both legacy and extended advertising features.
- Connection parameters
range
Defines the range of allowable connection parameters.
- Connection
roles
Defines the roles a device can assume in a BLE connection.
- Data status for extended
advertising reports
Defines the data status for extended advertising reports.
- Disconnect
reason
Defines the reasons for disconnection in the GAP (Generic Access Profile).
- Extended advertising data
operations
Defines the operations related to extended advertising data.
- Extended advertising event
properties
Defines the properties of extended advertising events.
- Event types for extended
advertising reports
Defines the event types for extended advertising reports.
- Event types of advertising
report
Defines the different types of BLE advertising report events.
- Extended primary advertising
interval range
Defines the range for the LE extended primary advertising interval in units of 0.625 ms.
- Extended scan data
length
Defines the range of extended scan data length.
- Extended scan
interval
Defines the range of LE extended scan intervals.
- Extended scan
window
Defines the range of LE extended scan windows.
- Fragment preference for
extended advertising data
Defines the preference on fragmenting extended advertising data.
- Initiator filter
policies
Defines the initiator filter policies.
- Maximum advertising data
length
Defines the maximum length of advertising data in bytes.
- Maximum advertising
handle
Defines the highest value that can be used as an advertising handle.
- Maximum advertiser list
size
Defines the maximum number of devices that can be included in the advertiser list.
- Maximum connection
handle
Defines the highest value that can be used as a connection handle in GAP (Generic Access Profile).
- Maximum device name
length
Defines the maximum length of a device name.
- Maximum extended advertising
data length
Defines the maximum length of extended advertising data in bytes.
- Maximum extended advertising
fragment data length
Defines the maximum length of extended advertising fragment data in bytes.
- Maximum filter accept list
size
Defines the maximum size of the filter accept list.
- Maximum number of
connections
Defines the maximum number of simultaneous GAP connections that can be maintained.
- Maximum number of skipped
periodic advertising events
Defines the maximum number of periodic advertising events that can be skipped.
- Maximum periodic advertising
data length
Defines the maximum length of periodic advertising data in bytes.
- Maximum periodic advertising
fragment data length
Defines the maximum data length for a single fragment of periodic advertising data.
- Maximum resolving list
size
Defines the maximum size of the resolving list.
- Maximum secondary
advertisements for extended scan
Defines the maximum number of secondary advertisements for extended scanning.
- Operation of periodic
advertising data
Defines operations related to periodic advertising data.
- Options for creating
synchronization
Defines the options for creating synchronization with a periodic advertising train.
- Options for enabling periodic advertising
Defines the options for enabling periodic advertising.
- Options for enabling periodic advertising train
Defines the options for enabling periodic advertising train.
- Path loss
zones
Defines the zones based on the level of path loss detected.
- Periodic advertising
interval
Defines the range of LE periodic advertising intervals.
- Periodic advertising
properties
Defines the properties of periodic advertising.
- PHY options for transmission
and reception
Defines the PHY options for transmission (TX) and reception (RX).
- PHY setting for extended
advertising reports
Defines the PHY settings for extended advertising reports.
- PHY type
Defines the PHY type for BLE connections.
- Preferred PHY coding
preference
Defines the preferred PHY coding for transmission on the LE Coded PHY.
- Privacy modes
Defines the privacy modes.
- Reasons for changing the address
Defines the reason for changing the address.
- Received data
status
Defines the status of received data in a BLE operation.
- RPA timeouts
Defines the Resolvable Private Address (RPA) timeouts.
- Scan channels
Defines the channel map bit field for scan.
- Scan filter duplicate
options
Defines the options for filtering duplicate advertising reports during scanning.
- Scan filter
length
Defines the maximum length of various scan filter fields.
- Scan filter
policies
Defines the scanning filter policies.
- Scan interval
Defines the range of LE scan intervals.
- Scan modes
Defines the scanning modes that determine the type of advertising packets that will be reported.
- Scan types
Defines the types of scanning methods that can be used.
- Scan window
Defines the range of LE scan windows.
- Status
definitions
Defines the various possible status.
- Subrate parameter range
Defines the range of allowable subrate parameters.
- Synchronization
timeout
Defines the synchronization timeout range for the periodic advertising train.
- The accuracy of the periodic
advertiser's clock
Defines the clock accuracy for periodic advertising.
- The transmit
power levels
Defines the flags for transmit power levels.
- Transmitter PHY
type
Defines the PHY types for transmitter test packets.
- TX power change
reason
Enumerates the reasons for reporting a change in TX (transmit) power.
- Type of constant tone
extension
Defines the type of Constant Tone Extension (CTE) used.
- LE Coded PHY options
Defines the Host preferred options when transmitting on the LE Coded PHY.