23.3.4.5 Timer/Counter Commands
The software can issue a command set to change the peripheral state immediately. These commands give direct control of the UPDATE, RESTART and RESET signals. A command is issued by writing the respective value to the Command (CMD) bit field in the Control E (TCEn.CTRLESET) register.
An UPDATE command has the same effect as when an UPDATE condition occurs, except that the UPDATE command is not affected by the state of the Lock Update (LUPD) bit in the Control E (TCEn.CTRLE) register.
The software can force a restart of the
current waveform period by issuing a RESTART command. In this case, the
counter, and all waveform outputs are set to ‘0’ .
A RESET command will set
all timer/counter registers to their initial values. A RESET command can
be issued only when the timer/counter is not running (ENABLE = 0 in the
TCEn.CTRLA register).