7 Known Issues

  • The library doesn’t set automatically the Update Source of the WEX module to the TCPWM0 option. The user has to set this option manually for the drive signals to be generated properly. Furthermore, the warning notification that instructs the user to do so will not disappear even if the action is completed.