1 Rationale
A system failure is produced by two types of faults: systematic and random.
Systematic faults, resulting from flawed hardware or a software implementation, can be mitigated through rigorously followed process control and an independent assessment. Design and implementation teams are separate from the assessment teams and are responsible for finding feasible solutions, while the assessment teams are tasked with finding possible implementation issues.
Random faults, on the other hand, cannot be anticipated or discovered through analysis during pre-deployment, therefore, the mitigation is limited to detection and eventually prevention. Random faults happen because of external factors that impact the system’s hardware.
Most systematic faults can be eliminated by redesigning during the testing phase, indicating that the system's safety level is directly related to the extent of mitigation of system random faults. As any system is not free of inherent, quantifiable failure rates with a probability always greater than zero, a system with a high level of SIL will always require switching to a Safe State when failure happens, through a planned mechanism (mitigation).
As a basic starting point, IEC61508 expresses the following view on risk:
- Zero risk is impossible.
- Non-tolerable (hazardous) risks must be always mitigated.
- The entire product life cycle (from design to decommissioning) must be covered.
Regardless of the standard that applies to a specific market, the safety integrity level is a function of level-of-risk reduction provided by an associated safety function, and represents the system probability of failure occurring before a system reaches a Safe State. In order to compare how different standards define the safety integrity level, one can use the probability of hazardous failures per time (billions of hours), or PFH, as a common reference (as presented below).
| IEC 61508 | IEC 62061 | ISO 13849 | ISO 26262 | DO 178B | Safety Level | |
|---|---|---|---|---|---|---|
| PFH | SIL | SILCL | PL | ASIL | DAL | |
| 10,000 ≤ PFH ≤ 100,000 | – | – | A | – | D,E | LOW
|
| 3,000 ≤ PFH ≤ 10,000 | 1 | 1 | B | – | C | |
| 1,000 ≤ PFH ≤ 3,000 | C | – | – | |||
| 100 ≤ PFH ≤ 1,000 | 2 | 2 | D | – | – | |
| 10 ≤ PFH ≤ 100 | 3 | 3 | E | B,C | B | |
| 1 ≤ PFH ≤ 10 | 4 | – | – | D | – | |
| PFH ≤ 1 | – | – | – | – | A | HIGH
|
Different standards offer different perspectives on how the safety integrity level is assessed and associated with a certain system. However, according to the presented table, a system complying with SIL 3 can be eventually recertified for ASIL C (ASIL B) or DAL B.
The failure risk mitigation usually increases the system complexity because of additional required checks. With this complexity increase, the overall reliability decreases, meaning that the safety level is not always a reliability-only related function. As an example, a two-out-of-two (2oo2) voting system, composed of two identical replicas (that agree on the decision) each with an associated 200 FIT (failure-in-time at a billion hours) rate, will have an equivalent of almost 400 FIT; this doubles the amount of failure rates because it is assumed that the two replicas will agree on the same decision and the probability of failure increases.
This can be somewhat confusing, as it appears that increasing design complexity is necessary to achieve the safety goal, which, in turn, may lead to reduced reliability. However, it is important to also consider the following:
- The goal is not to create a system with the highest possible reliability rate, but rather to reduce the number of dangerous system failures through effective processes and intelligent design.
- System modeling is not trivial, and the calculation and justification vary slightly across different standards, as there is no common model. However, the overall strategy remains the same.
To model the system for safety, the following failure behavior assumptions are in place:
- Failures always occur at constant rates (as being a Poisson process).
- Proof tests are assumed to be perfect and well-executed (a dangerous failure will not remain undetected).
- In systems with redundancy, failures in each channel are assumed to occur independently, with no common cause of failure.
The Industrial Safety standard IEC 61508 introduces the concept of synthesis/combining (section 7.4.3 of IEC 61508-2:2010). This strategic approach breaks down complex safety requirements into manageable (independent) components or subsystems. This method enables the achievement of a higher overall safety integrity goal by utilizing components with lower safety integrity levels, which are easier to attain.
When two elements are sufficiently independent, each possessing a systematic capability (SC) of N, their combination can be considered to have a maximum SC of N+1, where N equals 1, 2, or 3.
This translates into:
- SIL1 + SIL1 = SIL2
- SIL2 + SIL2 = SIL3
As for SIL 4 compliance, the standard mandates a multichannel implementation as the fault tolerance shall be greater than zero (see IEC 61508-2 chapters 7.4.4.3.1 and 7.4.4.3.2).
Sufficient independence at the hardware level between elements can be achieved by adopting the following strategies:
- Functional Diversity: use of different approaches to achieve the same results.
- Diverse Technologies: use of different types of equipment to achieve the same results.
- Common Parts/Services: ensuring that there are no common parts or services or support systems (for example, power supplies) whose failure could result in a dangerous mode of failure of all systems.
- Common Procedures: ensuring that there are no common operational, maintenance or test procedures.
The Automotive Safety standard ISO 26262 has a similar approach where safety requirements are broken down to redundant requirements and then allocated to independent Elements with Lower ASIL:
| Original ASIL | Possible ASIL Decomposition | ||
|---|---|---|---|
| ASIL D | ASIL C(D) + ASIL A(D) | ASIL B(D) + ASIL B(D) | ASIL D(D) + QM(D) |
| ASIL C | ASIL B(C) + ASIL A(C) | ASIL C(C) + QM(C) | — |
| ASIL B | ASIL A(B) + ASIL A(B) | ASIL B(B) + QM(B) | — |
| ASIL A | ASIL A(A) + QM(A) | — | — |
The automotive standard ISO 26262 introduces the concept of decomposition, a strategic approach that breaks down complex safety requirements into manageable, independent components or subsystems. The method allows for an efficient achievement of a higher overall safety integrity goal by using components with lower safety integrity levels.
Similarly, IEC61508 introduces the SIL synthesis concept, which is essentially equivalent to decomposition. It states that by combining elements with N systematic capabilities, a systematic capability of N + 1 up to SIL 3 can be achieved (see IEC 61508-2 chapter 7.4.3). For SIL 4 compliance, the standard mandates a multichannel implementation, as the fault tolerance shall be greater than zero (see IEC 61508-2 chapters 7.4.4.3.1 and 7.4.4.3.2).
To design such a complex system, the following points show how decomposition helps to achieve the objectives:
- Redundancy and Fault Tolerance: When a safety function is divided into multiple independent paths, the system continues operating due to redundancy, or the fault can be detected by comparing the results of the two paths, allowing for fault mitigation. Additionally, if the channels are independent, the probability that all channels will fail simultaneously is drastically reduced, because it involves multiplying the individual failure probabilities rather than adding them.
- Diagnostic Coverage and Safe Failure Fraction: Decomposition (or synthesis) allows for the integration of diagnostics that monitor the health of each channel through cross-checking, as simultaneous failures in two subsystems are unlikely. With high diagnostic coverage, dangerous failures are quickly detected, and the system is placed in a Safe State before the fault leads to a hazardous condition. This improves the Safe Failure Fraction, the proportion of failures that are either non-dangerous or detected before they lead to a hazardous event. Standards like IEC 61508 factor in SFF when setting SIL targets. Consequently, even if individual subsystems have moderate FIT values, enhanced diagnostics help ensure that undetected dangerous failures are far less likely.
- Failure Modes Isolation and Reduced Common-Mode of Failure: When the system is broken into robust, isolated modules, the chances that a single fault (or external event) will affect multiple channels simultaneously is minimized. This isolation means that the worst-case failure probability (which is what SIL is concerned with) is lower for the overall system versus the sum of its parts. In effect, careful decomposition (or synthesis) allows design engineers to mitigate Common-mode failures by ensuring that each redundant channel fails independently.
- Nominal Operational Conditions: Continuously monitoring external factors such as system power parameters and operating temperature ensure that subsystems do not operate outside nominal conditions, which could increase the likelihood of failure and invalidate any probabilistic assumptions about the system. If external extreme factors cannot be accurately predicted, component derating is employed as a mitigation technique.
The primary design goal of a safety system is to ensure that once a hazardous fault is detected, the system is transitioned to a Safe State, such as de-energized, stopped or stable. According to the railway standard EN 50129 Annex B, while hazardous events cannot be anticipated, they must be mitigated within a maximum amount of time called Safe Down Time (SDT), rendering the event harmless. in other words, SDT represents the maximum permissible duration for a safety function to remain non-operational. Alternatively, IEC 61508 defines Process Safety Time (PST) as a window of opportunity available to a safety function, from a hazardous failure occurrence until the moment the unmitigated process reaches a dangerous state.
It is more of a nuance than a difference, as PST addresses the system reaction in terms of speed and SDT addresses the duration during an outage (a safety function is missing or altered) without creating an intolerable risk.
By considering the focus on the system topology justification, PST is more suitable to be used instead of SDT, even if the two terms have slightly different meanings.
It is crucial to understand that the time required to transition the system to a safe state, taking into account all operational cycles, differs from the time needed to mitigate a fault at the subsystem level to prevent damage. Even if certain faults cannot be mitigated at the subsystem level, resulting in permanent damage due to the safety architecture by design, the system can still respond appropriately and return to a Safe State within the Process Safety Time (PST), achieving the safety goal.
For example, a safety electronic fuse must disconnect the load within a maximum of 10 ms (PST) to prevent a catastrophic failure. However, the subsystem responsible for short circuit detection and mitigation needs to perform its task within 2 µs (5000 times faster than PST) to disconnect the load without leading to permanent failure of the subsystem. If the subsystem that mitigates the short fails permanently, a supervisory subsystem can subsequently place the load in a safe state, such as de-energized, by using a pyrofuse or another air gap device within a more relaxed timeframe, such as 2 ms.
In the first case, if the subsystem responsible for short mitigation successfully fulfills its role and remains functional after mitigation, the load will be disconnected within 2 µs. Subsequently, the system within the Process Safety Time (PST), can attempt to reconnect to the load as a recovery mechanism, assuming the disturbance was transitory.
In the second case, if the subsystem fails to mitigate the fault and becomes damaged after 10 µs, for example, the supervisory system permanently disconnects the load through a secondary mechanism within 2 ms, with no further recovery. In both scenarios, the safety goal is achieved within the Process Safety Time (PST); however, the difference lies in whether the system experiences a temporary or permanent outage.
The following chapter demonstrates how the difference between the PST time requirement (10ms in this case) and functional fault mitigation time requirement (2 µs) makes the system design topology more flexible.