| AC PWM Generation | This example application shows how to
use the Analog Comparator Peripheral library to generate a 1 kHz PWM
waveform |
| AC Sleepwalking | This example application shows how to
use the AC Peripheral library to perform a single shot comparison in
standby sleep mode periodically and wake up the device at the end of a
successful comparison |
| ADC DMA Sleepwalking | This application shows how to
configure the ADC in a sleepwalking operation, where the input voltage
is measured at a fixed interval, and then the device is woken from sleep
after conversion of 16 samples |
| ADC Sample | This example application shows how to
sample an analog input using the ADC and displays the converted samples
on a serial terminal |
| ADC Window Sleepwalking | This application shows how to
configure ADC in a sleepwalking operation, where input voltage is
measured at a fixed interval, but device is not woken from sleep until
the measured value is below a given threshold |
| CCL Manchester Encoder | This example application shows how to
use the CCL peripheral library and generate a Manchester-encoded
output |
| Clock Configuration | This example application shows how to
configure the clock system to run the device at maximum frequency. It
also outputs a prescaled clock signal on a GPIO pin for measurement and
verification |
| DAC Waveform Generation | This example application shows how to
use the DAC to generate a 1 kHz Sine or Sawtooth wave with a look up
table |
| DAC Waveform Generation with DMA | This example application shows how to
use the DAC with the DMA to generate a 5 kHz sinusoidal waveform without
CPU intervention |
| DIVAS Accelerate Computations | This example application demonstrates
how to use the DIVAS accelerator to compute square root, and perform a
division and modulus operation |
| DIVAS Override C Division Operator | This example application demonstrates
how to override C division operator and modulus operator to use the
DIVAS accelerator |
| DMAC Memory Transfer | This example application demonstrates
how to use the DMAC peripheral to do a memory to memory transfer |
| DMAC USART Echo | This example application demonstrates
USART transfer with DMA to receive 10 bytes and echo back the received
bytes |
| DSU Compute CRC32 | This example application demonstrates
how to use the DSU Peripheral library to compute 32-bit Cyclic
Redundancy Checksum (CRC) |
| EIC Interrupt | This example application demonstrates
how to generate interrupt using the EIC on switch press and indicate it
through an LED |
| EVSYS Trigger | This example application demonstrates
how to use the EVSYS Peripheral library to setup autonomous, low-latency
and configurable communication between peripherals |
| FREQM Measurement | This example application demonstrates
how to use the FREQM peripheral to measure the frequency of the internal
RC Oscillator |
| NVMCTRL Data Flash | This example application demonstrates
code execution from the main Flash memory while performing erase
operation in data flash section |
| NVMCTRL Read Write | This example application demonstrates
how to use the NVMCTRL to erase and program the internal Flash
memory |
| PM Wakeup Using EIC | This application demonstrates
entering the low power modes and exiting it using the EIC |
| PM Wakeup Using RTC | This example demonstrates entering
the low power modes and exiting it using the RTC |
| PORT Polling | This example application demonstrate
how to poll the switch input, and indicate the switch status using the
LED |
| RSTC Reset Cause | This example shows how to use the
RSTC peripheral to indicate the cause of the device reset |
| RTC Alarm Interrupt | This example shows how to use the RTC
to configure the time and generate the alarm |
| RTC Periodic Interrupt | This example application shows how to
use the RTC to generate periodic interrupts |
| SDADC Sample | This example application shows how to
sample an analog input using SDADC and displays the converted samples on
a serial terminal |
| SERCOM I2C EEPROM Emulation (I2C
Slave) | This example application demonstrates
how to use the SERCOM peripheral in slave mode |
| SERCOM I2C EEPROM Read Write | This example application demonstrates
how to use the SERCOM peripheral to write and read from the I2C serial
EEPROM memory |
| SERCOM SPI EEPROM Read Write | This example application demonstrates
how to use the SERCOM SPI peripheral to write and read from the SPI
serial EEPROM memory |
| SERCOM SPI Interrupt | This example application shows how to
use SERCOM SPI PLIB with external loop back to write and then read back
an array of data in interrupt mode |
| SERCOM USART Interrupt | This example application demonstrates
how to use the SERCOM peripheral in USART mode to transfer data in a
non-blocking manner |
| Systick Periodic Interrupt | This example shows how to use the
SysTick to generate periodic interrupts |
| TC Capture Mode | This example shows how to use the TC
module in capture mode to measure duty cycle and frequency of an
external input |
| TC Compare Mode | This example shows how to use the TC
module in compare mode to generate an active low, active high, and
toggle output on compare match |
| TC Timer Mode | This example shows how to use the TC
module in timer mode to generate periodic interrupt |
| TCC PWM Generation | This example application shows how to
use the TCC to generate a 2 or 3 phase PWM signals for motor control
with dead time |
| TSENS Temperature Measurement | This example application shows how to
measure operating temperature of the device using the TSENS peripheral
and displays the measured temprature on a serial terminal. |
| WDT Timeout | This example shows how to generate a
Watchdog timer reset by emulating a deadlock |