4.2.3.1 diag_result_t
enum diag_result_t
Contains return codes for the diagnostic tests.
| DIAG_PASS | 0x81U - Indicates that no Fault was detected by the diagnostic | 
| DIAG_FAIL | 0x42U - Indicates that a Fault was detected by the diagnostic | 
| DIAG_INVALID_ARG | 0x24U - Indicates that the diagnostic was unsuccessful due to one or more invalid input arguments when calling the function | 
| DIAG_UNDEFINED | 0x7EU - Indicates that the result of the diagnostic is undefined due to incorrect usage of the API | 
| DIAG_NVM_STORE_ERROR | 0xBDU - Indicates that the Nonvolatile Memory (NVM) controller reported an error when attempting to write a value to nonvolatile memory | 
| DIAG_NOT_EXECUTED | 0x18U - Indicates that the test was not executed for the current run Note: 
 The enum values are chosen with a specific bit pattern to not overlap with the March diagnostic data backgrounds and avoid accidentally reporting an incorrect result. |