3 Interrupts
The stand-alone I2C module contains additional interrupt features designed to assist with communication functions. In addition to the MSSP module’s Start/Restart Condition (SCIF), Stop Condition (PCIF), Bus Collision (BCLIF), and transmit, receive, and acknowledge (SSPIF) interrupts, the stand-alone I2C module adds an Address Match (ADRIF), Transmit Buffer Empty (TXBE), Receive Buffer Full (RXBF), Bus Time-Out (BTOIF), Data Byte Count (CNTIF), Acknowledge Status Time (ACKTIF), and Not Acknowledge Detect (NACKIF).
The stand-alone I2C module incorporates a new register, the I2C Interrupt Flag register (I2CxPIR), which handles several I2C related interrupts. Additionally, when any of the Flag bits in I2CxPIR becomes set and the associated Interrupt Enable bits in the I2CxPIE register are set, the generic I2C Interrupt Flag (I2CxIF) is also set. If the matching Interrupt Enable bit is set, an interrupt is generated whenever the Interrupt Flag bit is set. If the appropriate Interrupt Enable bit is cleared, the Interrupt flag will still be set when the Interrupt condition occurs, however, no interrupt will be triggered.
The I2CxPIR contains the following Interrupt Flag bits:
- CNTIF: Byte Count Interrupt Flag
- ACKTIF: Acknowledge Status Time Interrupt Flag
- WRIF: Data Write Interrupt Flag
- ADRIF: Address Interrupt Flag
- PCIF: Stop Condition Interrupt Flag
- RSCIF: Restart Condition Interrupt Flag
- SCIF: Start Condition Interrupt Flag
The CNTIF becomes set (CNTIF = 1) when the I2CxCNT register
value reaches ‘0’, indicating that all bytes in the data frame have
been transmitted or received. CNTIF is set after the 9th falling edge of SCL when the
I2CxCNT = 0.
The ACKTIF becomes set (ACKTIF = 1) after the 9th falling edge of SCL
for any byte when the device is addressed as a client in any I2C Client mode
or I2C Multi-Host mode whenever an ACK is detected.
The WRIF becomes set (WRIF = 1) after the 8th falling edge of SCL when
the module receives a data byte. This bit is only active in any I2C Client
mode or I2C Multi-Host mode. Once the data byte is received, the WRIF is set,
as is the Receive Buffer Full (RXBF) Status bit, the I2C Receive Interrupt
Flag (I2CxRXIF) bit, and if the Data Write Interrupt and Hold Enable (WRIE) bit is set,
the generic I2CxIF bit is also set. The WRIF bit is read/write and must be cleared by
the user software, while the RXBF, I2CxRXIF, and I2CxIF are read-only, and are cleared
by reading the I2CxRXB.
The ADRIF becomes set on the 8th falling edge of SCL after the module has received either a matching 7-bit address byte or the matching upper or lower bytes of a 10-bit address. This bit is only active in Client mode or Multi-Host mode. Upon receiving a matching address byte, the ADRIF bit is set, and if the Address Interrupt and Hold Enable (ADRIE) bit is set, the generic I2CxIF bit is set.
The PCIF is set whenever a Stop condition is detected on the bus.
The RSCIF is set upon the detection of a Restart condition.
The SCIF is set upon the detection of a Start condition.
In addition to the I2CxPIR register, the stand-alone module incorporates the I2C Error register (I2CxERR). The I2CxERR register contains three Interrupt Flag bits that are used to detect bus errors. These bits are read/write and must be cleared by the user software. The I2CxERR register also includes the Enable bits for these three functions.
The I2CxERR register contains the following Interrupt Flag bits:
- BTOIF: Bus Time-Out Interrupt Flag
- BCLIF: Bus Collision Detect Interrupt Flag
- NACKIF: NACK Detect Interrupt Flag
The BTOIF is set when a bus time-out event occurs. The bus time-out time frame is
controlled by the I2C Bus Time-Out (I2CxBTO) register. If a bus time-out event occurs
and the module is configured as a client and is active (SMA = 1), BTOIF
is set, the SMA and CSTR bits are cleared, and the module is reset. When the BTOIF
becomes set and the Bus Time-Out Interrupt Enable (BTOIE) bit is set, the generic I2C
Error Interrupt Flag (I2CxEIF) bit is also set.
The BCLIF is set whenever a bus collision is detected. A bus collision occurs any time the SDA input is sampled low while both the SDA and SCL outputs are high. When a bus collision event occurs, the BCLIF becomes set, and if the Bus Collision Detect Interrupt Enable (BCLIE) bit is set, the generic I2CxEIF bit is also set.
The NACKIF is set when either the host or client is active (SMA = 1 ||
MMA = 1) and a NACK is detected on the bus. A NACK response occurs on
the 9th SCL pulse when the SDA line is released high. When the module is in Host mode, a
NACK can be issued when the host has finished receiving data from the client, or in the
event it did not receive a byte. In Client mode, the client issues a NACK when it does
not receive a matching address, or did not receive the last data byte. A NACK can also
be automatically sent if any of the following bits are set, which will set the NACKIF,
and if the NACK Detect Interrupt Enable (NACKIE) bit is set, the generic I2CxEIF is also
set:
- TXWE: Transmit Write Error Status bit
- RXRE: Receive Read Error Status bit
- TXU: Transmit Underflow Status bit
- RXO: Receive Overflow Status bit