1.30 RXLP Wakeup
This example application shows how RXLP can wakeup the device.
Description
Application starts by flashing the LED to indicate that it is powered up and running. Upon pressing the switch, it shutdowns the device(stops toggling the LED). When a character is sent over RXLP UART (from PC), the device will reset and run the application (starts toggling the LEDs).
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rxlp/wakeup/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a5d2_xult.X | MPLABX project for SAMA5D2 Xplained Ultra Evaluation Kit |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a5d2_xult.X | SAMA5D2 Xplained Ultra Evaluation Kit |
Setting Up SAMA5D2 Xplained Ultra Evaluation Kit
- SD Card with FAT32 file system
- Download harmony MPU bootstrap loader
- Copy the downloaded boot loader binary( boot.bin) onto the SD card
- SDMMC slot used for bootloading the application is SDMMC1
- Short jumper JP2 (DEBUG_DIS)
- Connect the Debug USB port on the board to the computer using a micro USB cable
- Connect the USB-UART click board to the computer using a mini USB cable
- Connect the USB-UART click board to the SAMA5D2-XULT board with the
following pin connections:
SAMA5D2-XULT pins USB-UART CLICK Pins J12, PIN 9 TX J12, PIN 11 GND
Running the Application
- Build the application using its IDE
- Copy the output binary (named ‘harmony.bin’) onto the SD Card (Refer to the ‘Setting up hardware’ section above for setting up the SD card)
- Insert the SD card into SDMMC slot on the board (Refer to the ‘Setting up hardware’ section for the correct SDMMC slot)
- Reset the board to run the application
- LED toggles indicating the board is up and running
- Press switch to shutdown the device (LED toggling stops)
- Configure USB-UART virtual COM port to operate with the following parameters (9600 baud, 8 bit data, no parity, 1 stop bit)
- Send a character on the USB UART Virtual COM port to reset the device
- Device resets (indicated by the LED starting to toggle again)
| Board | Switch Name | LED Name |
|---|---|---|
| SAMA5D2 Xplained Ultra Evaluation Kit | PB_USER | RGB_LED (Blue) |