2 Building AT91Bootstrap Project Using MPLAB X

  • Open a console and execute the following command to clone at91bootstrap repository into a directory named at91bootstrap.X
     git clone https://github.com/linux4sam/at91bootstrap at91bootstrap.X
  • Open at91bootstrap.X directory as project in MPLAB X

Configure Compiler

  • Open project properties window, and choose Makefile option to configure the compiler:
  • Default option is configured to use ARM gcc. To use xc32, replace all instances of arm-none-eabi- to xc32- as follows
Note: For the build to be successful, the configured compiler should be available in the system path.

Configure Target

  • Open project properties window, and choose Kconfig option to configure the build target:
  • Click the Load button and navigate to the configs folder inside at91bootstrap.X directory. The user needs to choose the default configuration file(defconfig) based on what the user needs the at91boostrap to do

    Debug/Run application from within MPLAB X

    • Load {evaluation_kit}_bkpt_none_defconfig. For example, on SAMA5D29 Curiosity Development Board, select sama5d2_curiosity_bkptnone_defconfig as the configuration file
    • Click Apply and OK buttons to configure the project
    • The user can see that the MPU product is selected as SAMA5D2 and the primary operation is selected as Configure and Stop

    Load and Run application from an SD card

    • Load {evaluation_kit}sd_uboot_defconfig. For example, on SAMA5D29 Curiosity Development Board, select sama5d29_curiositysd_uboot_defconfig as the configuration file
    • Click Apply and OK buttons to configure the project
    • The user can see that the MPU product is selected as SAMA5D2 and the primary operation is selected as Load and launch next software
    • Edit the Option Next Software Image File Name from u-boot.bin to harmony.bin

Build Target

Once the target configuration is applied in the properties window, the user can build the at91boostrap just as any other MPLAB X project. After the build is complete, the user can find the generated binary files under build/binaries directory.