12.8 INT Pin
The INT pin can be used to generate an asynchronous edge-triggered interrupt. This interrupt is
            enabled by setting the External Interrupt Enable (INTE) bit. The External Interrupt Edge Select (INTEDG) bit determines on which edge the interrupt will occur. When the
            INTEDG bit is set, the rising edge will cause the interrupt. When the INTEDG bit is
            clear, the falling edge will cause the interrupt. The External Interrupt Flag (INTF) bit will be set when a valid edge appears on the INT pin. If the GIE
            and INTE bits are also set, the processor will redirect program execution to the
            interrupt vector.