1.2 FAT File System using NVM Driver

This application shows an example of implementing a FAT disk in the device internal Flash memory.

Description

File System Operations on NVM:

Application places a FAT disk image consisting of a Master Boot Record (MBR) sector, Logical Boot Sector, File allocation Table, and Root Directory Area in the internal Flash memory (NVM). During execution, the application first opens an existing file named FILE.TXT and performs following file system related operations:

  • SYS_FS_FileStat
  • SYS_FS_FileSize
  • SYS_FS_FileSeek
  • SYS_FS_FileEOF

It tries to read the file and checks if string “Data” is present. If present it continues to next step or it fails the application. Finally, the string “Hello World” is written to this file. The string is then read and compared with the string that was written to the file. If the string compare is successful, An LED indication is provided.

File System Layer Uses:

  • Memory driver to communicate with underlying NVM media

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/fs/nvm_fat/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cm_jh01_curiosity_pro.XMPLABX project for PIC32CM JH01 Curiosity Pro Development Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32cm_jh01_curiosity_pro.XPIC32CM JH01 Curiosity Pro Development Board

Setting Up PIC32CM JH01 Curiosity Pro Development Board

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and program the application using its IDE
  2. Press Switch to start the file operations
  3. The LED is turned ON when the File “FILE.TXT” has the app data “Hello World” written in it
Refer to the following table for Switch and LED names:
BoardSwitch NameLED Name
PIC32CM JH01 Curiosity Pro Development BoardSW0LED0