1 Harmony 3 Driver and System Service Application Examples for SAM9X60 Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.
Name | Description |
---|---|
Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
FAT Filesystem throughput using SDMMC Media | This application calculates throughput by Writing and Reading data into a SD-Card at High Speed using the MPLAB Harmony File System and the SDMMC driver |
FAT Filesystem using RAM Media | This application shows an example of using the MPLAB Harmony File System to access RAM media |
FAT Filesystem using SDMMC Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDMMC driver |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
FreeRTOS Task Notification | This example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore |
I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
I2C Driver Synchronous - I2C EEPROM | This example application shows how to use the I2C driver in synchronous mode to perform operations on the EEPROM |
I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
SDMMC driver asynchronous - SDIO Read Write | This example application shows how to use the SDMMC driver in asynchronous mode to perform read/write operations using SDIO interface on the SD Card Media |
SDMMC Driver Asynchronous - SDMMC Read Write | This example application shows how to use the SDMMC driver in asynchronous mode to perform block operations on the SD Card Media |
SMC NAND Flash Driver - NAND Flash Read Write | This example application shows how to use the NAND Flash driver to perform read and write operations on NAND Flash device |
SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
USART Driver Asynchronous - USART Multi Instance | This example echoes the received characters over the two consoles using the USART driver in asynchronous mode |
USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |
USART Driver Synchronous - USART Multi Instance | This example echoes the received characters over the two consoles using the USART driver in synchronous mode |