8 Synchronous Initialization Example
The first step in initializing CryptoMemory ® is to determine what data will be stored in the device and what security settings are needed to protect this data. Once these are defined, determine the proper settings for the CryptoMemory registers and select values for the passwords. To initialize the CryptoMemory device, the following sequence is recommended and must take place in a secure location to protect sensitive data, passwords and keys that may be loaded into the device.