1.21 RTC Tamper Detect
This example application shows how to configure and use tamper detect feature of RTC.
Description
This example application shows how to setup system time and configure tamper detection using the RTC Peripheral Library. The application sets up system time and then waits for tamper detection to happen. On Tamper detection, application displays the tamper detected information and timestamp at which tamper is detected. Along with this, this example also demonstrates auto erase feature of backup register when tamper is detected. A known value is loaded into Backup register and displayed through console terminal. After tamper detection, it is evident that the pre-loaded value in backup register is erased.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rtc/rtc_tamper_detect/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_l10_xpro.X | MPLABX project for SAML10 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_l10_xpro.X | SAML10 Xplained Pro Evaluation Kit |
Setting Up SAM L10 Xplained Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the EDBG Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- System time is displayed in terminal session as RTC is configured in calendar
mode.
Note: System time value shown in the screen capture are for illustration purpose only. it will be updated every second while running the application. - To generate a tamper event, make the connection as follows:
Board Pad Connection Details SAML10 Xplained Pro Evaluation Kit PA08 EXT 1, Pin 14 to VCC and remove the connection to generate falling edge on RTC_IN0 (tamper event) Note: Using wires/jumpers may cause multiple detection because of connectivity glitch while shorting. - Upon detection of the tamper event, LED will be toggled and the console output
will be updated as follows:

| Board | LED Name |
|---|---|
| SAML10 Xplained Pro Evaluation Kit | LED0 |