4 Device Commands
- General Device
CommandsThese commands fall into two categories:
- General device access commands that are used to send data to the device or retrieve data but typically do not perform any cryptographic functions
- General cryptographic commands that can be used by the device or the system but typically do not operate on specific data slots
- Asymmetric Cryptography
Commands
These commands perform asymmetric cryptographic operations, such as key generation, message signing and message verification that utilize an ECC public or private key. These commands are limited to use on ECC Data zone slots.
- Symmetric Cryptography
Commands
These commands perform a symmetric cryptographic function, such as generating a digest or MAC, key derivation or AES encryption and decryption.
Input Parameters for All Commands
The multibyte input parameters display as big-endian (MSB first) values in the input parameters tables, unless otherwise specified. Note that the ECC608-TFLXWPC device actually expects the data to be sent little-endian (LSB first).
| Command | Description | Command Category |
|---|---|---|
Counter | Reads or increments one of the monotonic counters | General Device Commands |
ECDH | Generates an ECDH pre-master secret using stored private key and input public key | Asymmetric Cryptography Command |
GenKey | Generates an ECC public key. Optionally generates an ECC private key | Asymmetric Cryptography Command |
Info | Returns device state information | General Device Commands |
Lock | Prevents further modifications to a zone or slot of the device | General Device Commands |
Nonce | Generates a 32-byte random number and an internally stored Nonce | General Device Commands |
Random | Generates a random number | General Device Commands |
Read | Reads 4 or 32 bytes from the device, with or without authentication and encryption | General Device Commands |
SecureBoot | Validates code signature or code digest on power-up | Asymmetric Cryptography Command |
SelfTest | Tests the various internal cryptographic computation elements | General Device Commands |
Sign | ECDSA signature calculation | Asymmetric Cryptography Command |
SHA | Computes a SHA-256 or HMAC digest for general purpose use by the system | General Device Commands |
UpdateExtra | Updates bytes 84 or 85 within the Configuration zone after the Configuration zone is locked | General Device Commands |
Verify | ECDSA verify calculation | Asymmetric Cryptography Command |
Write | Writes 4 or 32 bytes to the device, with or without authentication and encryption | General Device Commands |