9.7 Resolved Issues
(Ask a Question)The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2022.2 that have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Case Number | Summary | Resolution |
|---|---|---|
| 00910093 | MPF Programming issue with Zeroize and Authentication
PROC_ENABLE. | ENC_DATA_AUTHENTICATION,
ZEROIZE_LIKE_NEW, and ZEROIZE_UNRECOVERABLE
actions now pass for exported bitstream file/FlashPro Express job when
include plaintext passkey is checked and these actions are
disabled in the Configure Security tool. |
| 122358 | If the PolarFire CCC is configured in Post-Divider Feedback Mode, the phase shift continuously changes after power cycling the device (Core Version 2.2.100). | For information, see section PLL Phase Alignment when Using Post-Divider or External Feedback Mode. |
| 00998202 | The vdir command used with ModelSim ME Pro
2021.3 for pre-compiled libraries delivers the incorrect result of unknown
version. | This issue is resolved with the ModelSim ME Pro provided with Libero v2022.2. |
|
493642-2872943656, 493642-2880122269, 00850681 | RTG4_CCC: Simulation of RTG4 Design using a FCCC PLL with external feedback: phase delay is not adjusted. | For information, see section Added Simulation Support for RTG4 PLL Feedback Delay. |
| 00967580 | RTG4_ODT: Dynamic ODT macro simulation library bug. | The ODT_DYNAMIC simulation model has been
updated to match the port names with libero generated files. |
| — | A deadlock condition with the RTG4FCCCECALIB core occurred when configured for external feedback mode and output option-1 to hold the outputs LOW until the lock asserts. | If External Feedback is selected and the
FB_CLK source is one of the CCC's GLx outputs, your CCC output setting of Hold outputs
LOW until PLL locks is ignored for the GLx that is sourcing the
FB_CLK and that GLx is allowed to operate prior to lock
assertion. |
| — | When setting permanently write protect fabric in Configure Permanent Locks tool, the exported bitstream file/job will also program sNVM update protection to be locked for update (i.e., protected by Flashlock/UPK1) even though sNVM updates were allowed without Flashlock/UPK1 in Configure Security tool. | Security settings for Fabric and sNVM can now be saved or read separately. |
| — | Installing Libero SoC v2022.1 on a Personal Computer (PC) running windows causes the PC to restart unexpectedly without providing a notification message. | To avoid this issue, install Visual C++ Redistributable 2015-2022 x86 on the PC before installing Libero SoC v2022.1. |
| 01037234 | Stage3 Initialization Client data of the Golden and Update images is not available in the exported SPI Flash image. | The Export SPI Flash Image tool now exports data for STAGE3 initialization client imported via SPI Bitstream client in the SPI-Flash tab of the Configure Design Initialization Data and Memory tool. |
| 912639 | HDL_LANGUAGE: VHDL: Libero is not parsing files correctly to pass to Synthesis. | Libero is not parsing the dependent package files correctly to pass to Synthesis. |
| 967427 | G4: Sanitize option is increasing stpl file size unexpectedly. | Generate Bitstream, Export Bitstream, and Export FlashPro Express Job tools do not unnecessarily include entire fabric data when sanitizing eNVM as part of an ERASE action. |
|
493642-2092580450, 493642-2707760243 | Add information for update_and_run_tool in the
Libero online help. |
A tool state can be Out of Date (OOD) for various reasons, such as when there is a change in the source files, a change in settings, a parent tool state cleaned, or out-of-date. If a tool is out of date, the |
| 493642-2868126969 | COMPONENT_MANIFEST: Include SDC in manifest text files of SmartDesign generated Core IPs. | For information, see section Constraint Files in the Manifest Text Files of Generated Core IPs. |
| 964688 | Update the Libero SoC Linux Environment Setup User Guide . | The wizard for installing Libero SoC v2022.2 has been streamlined and simplified while allowing you to control what gets installed. |
| 00938240, 00972272 | If reserve pins for probes is unselected, System Controller suspend mode is unavailable. | When configuring programming options, the Disable probe read/write option depends on a Constraints Manager option that reserves pins for the probe. If the reserve pins for probe option are not selected, probe read/write must be disabled and cannot be changed. Default for the disable probe read/write is based on the current reserve pins for probe setting: off and available for you to change if pins reserved or on and unchangeable if pins are not reserved. |
| 939458 | Add a popup when discrete clock is selected in the Programmer Settings dialog. | In addition to adding a pop-up warning in the Programmer Settings dialog, a warning is added when you perform a Program, Verify, Erase, or Authenticate action to advise you about significant programming time increase in case the discrete clock mode is set for the selected programmer |
| 910093 | FlashPro 6 turbo (SPI-Slave): MPF Programming issue with Zeroize and Authentication PROC_ENABLE. | Added zeroization support for secured devices. |
| 906419 | KIT_LICENSE_IP: Gold License has an issue with Mi-V running on MPF300T. | Close and reopen the Libero project. |
| 959171 | KIT_LICENSE_IP: The CoreUARTapb v5.7.100 FIFO depth has an issue with the gold license. | Close and reopen the Libero project. |
| 493642-2784815561 | PF_PCIE: PF_CRYPTO: DRC check for PCIe and Crypto configurator when the clock frequencies are between 70 to 125 MHz. | Confirmed that in PolarFire SoC designs, DRC checks for PCIe and Crypto configurator when clock frequencies are between 70 and 125 MHz. |
| 493642-2695344599 | RTG4_CCC:CCC Core Generation is failing for some Lock Window values. | The RTG4FCCC and RTG4FCCECALIB cores are updated to show DRC for unsupported ppm values. |
| 886516 | Place and Route Globals Assigner failure with MPFS250T-FCSG536E device. | Select the appropriate pin type that can drive GBs or PLLs as needed, and then use the INBUF+CLKINT solution and have IO Bank Assigner infer a hardwired connection if available. |
| 860917 | PF_IOD_GENERIC_RX Fabric Global Clock from external Source. | Updated RX_CLK_G and
RX_CLK_TO_PLL ports visibility in symbol view. |
| 941837 | RTG4FCCC/RTG4FCCCECALIB: Expose GLx_Yx_ARST_N in CCC configurator GUI. | For information, see section Changing Default Behavior of GLx_Yx_ARST_N Signals in the CCC Configurator. |
| 968882 | Repair min delay affects max timing closure. | Automatically generated clock jitter does not impact min-delay timing. |
| 878534 | STPS-373 - SmartTime in v2021.2 considers invalid false path constraint. | Applied false path constraints now work properly and warnings about invalid false path constraints no longer appear. |
| 904319 | STPS-381 - Constraint Editor GUI column width issue in Libero v2021.2 and v2021.3. | The constraint browser pane on the left side can now be reduced and increased without issues or standard column width. |
| 1001850 | Clock generation value is 0 ns for muxed clocks in Libero v2022.1. | Fix SmartFusion2/IGLOO2 zero clock generation delay for muxed clocks. |
| 868286 | PF_SOC: MSS: Warning if MSS_QSPI and SPI I/O config is split between MSSIO and Fabric. | The PolarFire SoC MSS Configurator is updated to print a warning message if the QSPI/SPI peripherals are split between MSSI/Os and Fabric I/Os. |
| 980695 | PolarFire Post Compile does not route the N pins of the differential Buffer. | The OUTBUF_DIFF_IOG and
TRIBUFF_DIFF_IOG macros have been updated to include the connection
from the IO to IOPADN for the E and D pins. |
| 998202 | ModelSim ME Pro 2021.3 PC version only - vdir
command is giving results as unknown version. | This issue is resolved with the ModelSim ME Pro provided with Libero v2022.2. |
|
00907718, 00987912 | Create_generated_clock issues warning. | This issue is resolved with the ModelSim ME Pro provided with Libero v2022.2. |
| 493642-2820955992 | IBIS model of the I2C Component of Airbus issue. | For BIDIR pins, both Input and Output IBIS models are exported. |
| 950237 | The IBIS modes for the LVDS inputs for RTMPF are not getting generated. | LVDS Input side IBIS models are generated as expected for RTPF device. |
| 971142 | SmartTime and PnR Jitter report has 25 ns as jitter for the
PLL_OUT3 clock. | Changed the jitter value for PLL output to cap at 16.667 ns when the frequency is lower than 1.5 MHz. |
| 996553 | M2S MDDR and FDDR register initialization compared to the RTG4 FDDR initialization. | The IGLOO2 FDDR Core ABC Register initialization is now similar to RTG4 FDDR. |
| 493642-2771429137 | SmartFusion2 eNVM1 remap defeature. | For information, see section Prevent Remapping Data from eNVM_1 Memory Block to Cortex-M3 Code Space. |
| 959860 | PF_XCVR: XCVR configurator incorrectly setting register bit. | Add the PMA_CTRL_RO register value after all the
registers are processed at the end of the assembly file, and then use the MODE2 option
to generate the mem file and bitstream. |
| — | For PolarFire SoC Libero designs that contain eNVM, running VERIFY_DIGEST after programming device fails with the message eNVM digest verification: FAIL. | The eNVM client in Configure Design Initialization Data and Memories tool has a new option to include pages for digest calculation, which resolves this issue. See section eNVM Client Digest Option. |
The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2022.2 that do not have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Summary | Resolution |
|---|---|
| Timing analysis reports same path twice. | Verified that all paths are reported for the clock domain and that the clock domain for CCC output is not created. |
| PF TAMPER macro outputs need latching when using System Controller Suspend mode | For information, see section PF_TAMPER Enhancement to Latch Outputs when Using System Controller Suspend Mode. |
| Add support in TCL for location coordinates for each element instantiated in canvas. | Added the new option in the Export Component Description (TCL)
dialog to also export SmartDesign presentation model. Exported presentation model
(*.pm) files can be used to recreate SmartDesign presentation by
the newly added sd_apply_presentation TCL command. |
| New Flash device support: IS25LP128 from ISSI vendor. | Add programming device support of IS25LP128 with FlashPro 6. |
| Developer mode GUI option is not intuitive. | The Create New Job Project dialog has more information about how to create a new project in case you do not have a job file and how to switch to developer mode. The current mode, operator, or developer is always shown in the FlashPro Express title. |
| PF_CCC: PLL_LOCK configuration missing. | For information, see section PLL Phase Alignment when Using Post-Divider or External Feedback Mode. |
| PF_CCC: Backup clock is not supported in External and Post-Divider Feedback Mode. | For information, see section PLL Phase Alignment when Using Post-Divider or External Feedback Mode. |
| PF_CCC: Reset on lock in Post-VCO Mode. | For information, see section PLL Phase Alignment when Using Post-Divider or External Feedback Mode. |
| SmartPower crashes while exporting MPE report. | Added condition to handle null values while exporting MPE report. |
| SSN Analyzer: DEF0012: Unable to open file SSNAnalyzer.def: line 56: 20245 Segmentation fault. | Exported the file to the staging area. |
Add THIS FILE IS AUTO GENERATED DO NOT MODIFY
statement in derived constraint file. | A message now appears if modifications to a derive constraints file will be lost. |
| Incorrect violations reported in constraint coverage. | Setup violations in coverage reports are zero when report violations have zero violations. |
| PF_SOC: MSS: Point out to users that scratchpad memory for HSS/Linux systems. | To ensure that sufficient scratchpad memory is allocated to the
bootloader using the L2 Cache tab, a warning message now
appears if SCRATCHSIZE is less than 4 (512 KB) in GUI and batch
mode. |
| PF_SOC: MSS: MSS missing the port BOOT_FAIL. | Added an Expose Boot Status ports check
box that, when checked, exposes the BOOT_FAIL_CLEAR_F2M and
BOOT_FAIL_ERROR_M2F ports to users. |
| PF_SOC: MSS: MSS_I2C - Fabric Interface missing inverter for open drain I/O. | If fabric is selected for I2C for production device, inverters
have been added for the following ports:
|
| RTG4 CCC/PLL: Clock Uncertainty: RTG4 CCC/PLL must also derive clock jitter constraints per DS jitter specification. | For information, see section New Timing Constraint Flow Accounts for Global Clock Jitter Automatically . |
| Libero does not generate IBIS models for PolarFire EXT temp grade. | EXT temperature range supported for IBIS. |
| Export Job Manager data step does not include information about back-level bypass. | Added an option for bypassing back-level protection for Recovery/Golden bitstreams. The selected setting is saved in the JDC file and passed to the Job Manager. |