6 M-HSM Server Replication
An existing M-HSM server can be replicated to one or more new M-HSM servers. As a result, the replicated server gets a copy of the Security World, all HSM keys, imported public keys, the DFK DB, and the manufacturing keys already existing on the source system.
Note: Programming jobs cannot be replicated, but they can be transferred. The overbuild
protection does not allow cloning of any job that may exist in the source system. Job
tickets reside inside the physical HSM module, and can only be transferred to the new
system along with the physical module.
The following sections provide instructions for M-HSM server replication.