4.1 Getting Started with MCHPRT3
MCHPRT3 Package Features
- RF – RF Test for Bluetooth and Zigbee TX/RX
- Calibration – TX Calibration and RX Calibration
- MAC Address – Read/Write Bluetooth Address and Zigbee MAC Address
- Information Block (IB) File – Read/Save IB File to/from Buffer and Read/Commit IB Buffer to/from DUT
- GPIO – GPIO Test Command
The following are the steps to launch the MCHPRT3 tool:
- Double click
MCHPRT3.exeunder direction:C:\Microchip\MCHPRT3_Setup_v1.0.1.XXXX; the following screen appears.Figure 4-3. Start-Up Window of the MCHPRT3 Tool - From the “Select GUI” drop-down list, select PIC32CX-BZ36.
- Click Open to launch the PIC32CX-BZ36 window (see the following figure).
Description of each component:
- Buttons on the top:
- Connect/Disconnect – Connects or disconnects the PIC32CX-BZ36
- Reset – Reset the PIC32CX-BZ36
- Refresh COM – Update the list of connected com port
- Cal. VCO – VCO calibration
- BUCK PWM – Switch the power mode into DC-DC (Buck) mode
- PMU MLDO – Switch the power mode into MLDO mode
- Get FW Version – Obtain the firmware version from the sample
- Enable PKOB4 – Only needed to check if the user is using the PIC32CX-BZ36 Curiosity Board
- RF for Bluetooth and Zigbee –
Settings of RF mode, channel and TX parameter for RF test
- BT – TX setting of payload, PHY (data rate), packet length and power step (power level). RX – number of RX packet.
- Zigbee – TX settings of packet type, power level, delay time between each packet and packet number. RX – setting of RX data rate and number of RX packet.
- Calibration – Complete TX and RX
calibration flow. The user can save calibration info to file or commit to NVM type
Flash or OTP.
- TX Calibration – Perform TX calibration flow to adjust transmitted power and output frequency to target.
- RX Calibration – Perform RX calibration flow to obtain RX IQ, RSSI to corresponding received power and so on.
- MAC Address – Read/write address
- BT address and Zigbee MAC address
- IB (Information Block) File
- Read IB file to IB buffer/save IB buffer to IB file
- Read DUT to IB buffer/commit IB buffer to DUT
- GPIO – Test GPIO for selected port,
pin, in/out and level
- Start GPIO – Initialize GPIO for test
- GPIO Command – Execute GPIO test command for selected port, pin, in/out and level
- Stop GPIO – Stop GPIO test