2.10.1 Windows®
When installing the Atmel-ICE on a computer running Microsoft® Windows®, the USB driver is loaded when the Atmel-ICE is first plugged in.
Note:
Be sure to install the front-end software packages before plugging the unit in for the first time.
Once successfully installed, the Atmel-ICE will appear in the device manager as a "Human Interface Device".