29.6.10 Status

Name: STATUS
Offset: 0x1A
Reset: 0x0000
Property: –

Bit 15141312111098 
          
Access  
Reset  
Bit 76543210 
  TXECOLLISFCTSBUFOVFFERRPERR 
Access RR/WR/WRR/WR/WR/W 
Reset 0000000 

Bit 6 – TXE Transmitter Empty

When CTRLA.FORM is set to LIN Host mode, this bit is set when any ongoing transmission is complete and TxDATA is empty.

When CTRLA.FORM is not set to LIN Host mode, this bit will always read back as zero.

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit will clear it.

Bit 5 – COLL Collision Detected

This bit is cleared by writing ‘1’ to the bit or by disabling the receiver.

This bit is set when collision detection is enabled (CTRLB.COLDEN) and a collision is detected.

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit will clear it.

Bit 4 – ISF Inconsistent Sync Field

This bit is cleared by writing ‘1’ to the bit or by disabling the receiver.

This bit is set when the frame format is set to auto-baud (CTRLA.FORM) and a sync field not equal to 0x55 is received.

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit will clear it.

Bit 3 – CTS Clear to Send

This bit indicates the current level of the CTS pin when flow control is enabled (CTRLA.TXPO).

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit has no effect.

Bit 2 – BUFOVF Buffer Overflow

Reading this bit before reading the Data register will indicate the error status of the next character to be read.

This bit is cleared by writing ‘1’ to the bit or by disabling the receiver.

This bit is set when a buffer overflow condition is detected. A buffer overflow occurs when the receive buffer is full, there is a new character waiting in the receive shift register and a new start bit is detected.

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit will clear it.

Bit 1 – FERR Frame Error

Reading this bit before reading the Data register will indicate the error status of the next character to be read.

This bit is cleared by writing ‘1’ to the bit or by disabling the receiver.

This bit is set if the received character had a frame error, i.e., when the first stop bit is ‘0’.

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit will clear it.

Bit 0 – PERR Parity Error

Reading this bit before reading the Data register will indicate the error status of the next character to be read.

This bit is cleared by writing ‘1’ to the bit or by disabling the receiver.

This bit is set if parity checking is enabled and a parity error is detected.

Writing ‘0’ to this bit has no effect.

Writing ‘1’ to this bit will clear it.