4.4.3 SRAM Quality of Service

To ensure that hosts with latency requirements receive sufficient priority when accessing SRAM, the different hosts can be configured to have a given priority for different types of access.

The Quality of Service (QoS) level is independently selected for each host accessing the SRAM. For any access to the SRAM, the SRAM also receives the QoS level. The QoS levels and their corresponding bit values for the QoS level configuration is shown in the following table.

Table 4-7. Quality of Service Level Configuration
ValueNameDescription
0x0DISABLEBackground (no sensitive operation)
0x1LOWSensitive Bandwidth
0x2MEDIUMSensitive Latency
0x3HIGHCritical Latency

If a host is configured with QoS level DISABLE (0x0) or LOW (0x1), there will be a minimum latency of one cycle for the SRAM access.

The priority order for concurrent accesses is determined by two factors: First, the QoS level for the host, and second, a static priority given by the SRAM Port ID, as defined in SRAM Port Connections. The lowest port ID has the highest static priority.

The MTB has a fixed QoS level of HIGH (0x3).

The CPU QoS level can be written to or read from address 0x4100A110, bits [1:0]. Its reset value is 0x0.

Refer to the different host registers for configuring their QoS.