4.3.2 Use Data Visualizer Streamer to See the Classification

  1. Launch MPLAB Data Visualizer.
  2. Configure Data Visualizer.
    1. Click Load.
      Figure 4-14. MPLAB® Data Visualizer
      ???
    2. Find and open the file predictive_maintenance_demo.dvws within the dv-workspace folder on the companion material.
      Figure 4-15. MPLAB® Data Visualizer Workspace Configuration File Selection for Motor State Classification
      ???

      The following screen will appear.

      Figure 4-16. MPLAB® Data Visualizer Project Workspace Properly Loaded
      ???
  3. Select the COM port used by the PKoB.
  4. Click the MCU Reset button (SW4) on the board.
  5. Data Visualizer will show the current motor state, which should be OFF.
    Figure 4-17. MPLAB® Data Visualizer Workspace Properly Connected to the Device
    ???
  6. Press the SW1 button to start the motor.
  7. Confirm the motor runs and the Data Visualizer indicates Normal operation.
    Figure 4-18. MPLAB® Data Visualizer Indicating Normal Operation
    ???