3.3 Measuring Effective Load Capacitance
The crystal frequency is dependent on the capacitive load applied, as shown by Equation 1-2. Applying the capacitive load specified in the crystal data sheet will provide a frequency very close to the nominal frequency of 32.768 kHz. If other capacitive loads are applied, the frequency will change. The frequency will increase if the capacitive load is decreased and will decrease if the load is increased, as shown in Figure 3-9.
The frequency pull-ability or bandwidth, that is, how far from the nominal frequency the resonant frequency can be forced by applying load, depends on the Q-factor of the resonator. The bandwidth is given by the nominal frequency divided by the Q-factor, and for high-Q quartz crystals, the usable bandwidth is limited. If the measured frequency deviates from the nominal frequency, the oscillator will be less robust. This is due to higher attenuation in the feedback loop β(jω) that will cause a higher loading of the amplifier A to achieve unity gain (see Figure 1-2).
A good way of measuring the effective load capacitance (the sum of load capacitance and parasitic capacitance) is to measure the oscillator frequency and compare it to the nominal frequency of 32.768 kHz. If the measured frequency is close to 32.768 kHz, the effective load capacitance will be close to the specification. Do this by using the firmware supplied with this application note and a standard 10X scope probe on the clock output on an I/O pin, or, if available, measuring the crystal directly with a high-impedance probe intended for crystal measurements. See Section 4, Test Firmware, for more details.
Equation 3-4 gives the total load capacitance without external capacitors. In most cases, external capacitors (CEL1 and CEL2) must be added to match the capacitive load specified in the crystal’s data sheet. If using external capacitors, Equation 3-5 gives the total capacitive load.