1.7 FreeRTOS Task Notification

This example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore.

Description

  • This demonstration creates two tasks that send notifications back and forth to each other.
    • Task2 blocks to wait for Task1 to notify and will be blocked for 500ms
    • Task1 sends a notification to Tasks2, bringing it out of the blocked state, toggles an LED
    • Task1 blocks to wait for Task2 to notify
    • Task2 sends notification to Task1, bringing it out of the blocked state
  • Above steps will be repeated. i.e.: an LED toggles for every 500ms

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/rtos/freertos/task_notification_freertos/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mx470_curiosity.XMPLABX project for Curiosity PIC32MX470 Development Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mx470_curiosity.XCuriosity PIC32MX470 Development Board

Setting Up Curiosity PIC32MX470 Development Board

  • Connect mini USB cable to the ‘Debug USB’ connector(J3) on the board to the computer

Running the Application

  1. Build and program the application using its IDE
  2. The LED toggles on success for every 500ms
Refer to the following table for LED name: