5 Interrupt on VDDIO2 Status
When the state of the VDDIO2 Status bit changes, the VDDIO2 interrupt flag will be raised. To be able to catch this interrupt immediately, it is necessary to enable both the VDDIO2 interrupt and global interrupts in general.
/*Enable the VDDIO2 interrupt*/ MVIO.INTCTRL |= MVIO_VDDIO2IE_bm; /*Enable Global interrupts*/ sei();
The MVIO vector will be called when the interrupt is triggered. Before returning from the
Interrupt Service Routine (ISR), the VDDIO2 (VDDIO2IF) interrupt flag in the MVIO
Interrupt Flags (MVIO.INTFLAGS) register must be cleared. This is done by writing a
‘1’ to the flag.
ISR(MVIO_MVIO_vect)
{
/* The VDDIO2 interrupt has been triggered */
LED0_toggle();
/* Clear the CFD interrupt flag */
MVIO.INTFLAGS |= MVIO_VDDIO2IF_bm;
}