7.5 Demo Operation
- Connect the hardware and prepare the demonstrator setup, following the instructions provided in the Demo Setup section.
- Configure the data visualizer, following the instructions provided in the Data Visualizer Configuration section.
- Click the Serial Port Control Panel Connect button.
- Click the SW0 button on the Curiosity Nano board and select the appropriate frequency for the three-phase signal. The selected frequency is displayed on the custom dashboard window.
- Zoom in or out the graph on the Graph window by clicking the +/- magnifier symbol below the Graph window.
- Insert phase loss fault by clicking the L1 radio button on dashboard, which disables the L1 signal out of three-phase signal to emulate phase loss input. Figure 7-15 shows the three-phase signal with L1 phase-loss fault and the L1 phase-loss status indicator on the dashboard.
- Insert phase loss fault by clicking the L2 radio button on dashboard, which disables the L2 signal out of three-phase signal to emulate phase loss input. Figure 7-16 shows the three-phase signal with L2 phase-loss fault and the L2 phase-loss status indicator on the dashboard.
- Insert phase-loss fault by clicking the L3 radio button on the dashboard, which disables the L3 signal out of three-phase signal to emulate phase-loss input. Figure 7-17 shows the three-phase signal with L3 phase-loss fault and the L3 phase-loss status indicator on the dashboard.
Insert phase-reversal by clicking the PR radio button on the dashboard, which changes the sequence of the three-phase signal to L1-L3-L2. Figure 7-18 shows the phase-reversal input and phase-reversal status indication on the dashboard.
- Observe the RMS voltage of the three-phase signal on the dashboard
Refer to the User Inputs section for more information about user input.