3.2 Foundation Services Generated Code
To generate this project using the Foundation Services library, follow these steps:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open the MCC from the toolbar (information on how to install the MCC plug-in can be found on the Microchip website).
- Go to Project
Resources > System > System Module and
use the following configurations:
- Oscillator Select: HFINTOSC
- HF Internal Clock: 4 MHz
- Clock Divider: 4
- In the WDT Enable field, in the WWDT tab, ensure WDT Disable is selected
- In the Programming tab, make sure Low-Voltage Programming Enable is checked
- In Device Resource, under Libraries, find Foundation Services, expand it and double-click UART to add it to the project.
- Click the + button at the bottom to add a new Foundation Services federated UART.
- Select EUSART2 from the UART drop down in Foundation Services.
- Open the Pin
Manager > Grid View window, select
UQFN40 in the MCU package field and select pin
RD0 EUSART TX.
Figure 3-2. Pin Mapping - In Project Resources,
under Peripherals, select EUSART2 and use the following
configuration:
- Redirect STDIO to USART: Checked
- Click Generate in the Project Resources tab.
- In the
main.cfile, which was generated by MCC:- Uncomment the line that enables global interrupts and the one that enables peripheral interrupts
- Add the
following
defines:
#define START_DATA_STREAM_PROTOCOL 0x03 #define STOP_DATA_STREAM_PROTOCOL 0xFC
- Add the
following code in the main function (replacing the
existing
while(1)loop):uint8_t cnt = 0; while (1) { printf("%c%c%c%c", START_DATA_STREAM_PROTOCOL, cnt, cnt * 2, STOP_DATA_STREAM_PROTOCOL); cnt = cnt + 1; __delay_ms(50); }
- Use MPLAB X Data Visualizer as described in the appendix, How to configure MPLAB X Data Visualizer to Decode Data Stream Protocol.