5.1.2.2 Info - KeyValid

The KeyValid mode is useful to determine if an ECC private or public key that is stored is a valid ECC key. If the PublicKey cannot be output, then the info returned by this command is not useful. If the KeyType is not ECC, the output of this command is also not useful.

For the ATECC608A-TFLXTLS device, the keys stored in Slots 0-4, 11 and 13-15 are ECC keys that can be checked with the KeyValid mode of the Info command.

Table 5-7. Input Parameters - Info KeyValid

Opcode
(1 Byte)

Mode
(1 Byte)

Param
(2 Bytes)

Data
(0 Bytes)

Description
0x300x010x00 0[Slot]—Returns whether the slot contains a valid ECC private or public key.
Table 5-8. Output Response - Info KeyValid
Name

Size
(4 Bytes)

Description
Response0x00 00 00 00ECC key is invalid
0x00 00 00 01ECC key is valid