5.1.2.4 Info - Write GPIO Output

The SWI device version of the ATECC608A-TFLXTLS has a single GPIO pin configured as an output buffer. The output will default to a LOW value upon device power-up. The value of this output can be changed by using the INFO Command in GPIO Write mode.

Note: This command is only available for the SWI devices and can not be used with I2C devices

Upon successful completion the command will return a four byte response with the LSB indicating the value that the output was written to. If the command fails then a single error code byte will be returned.

Table 5-12. Input Parameters - Info GPIO Output Write

Opcode
(1 Byte)

Mode
(1 Byte)

Param
(2 Bytes)

Data
(0 Bytes)

Description
0x300x030x00 02—Write a value of Zero to the GPIO Output
0x030x00 03—Write a value of One to the GPIO Output
Table 5-13. Output Response - Info GPIO Output Write
NameResponseDescription
Response0x00 00 00 00Successful return value if GPIO has been written to a 0
0x00 00 00 01Successful return value if GPIO has been written to a 1
0xXXSingle Byte Error code upon failure