| ADC Polling | This
example demonstrates how to sample an analog input in polled mode
and send the converted data to console |
| ADC User Sequence | This
example demonstrates how to sample three analog inputs using the
user sequencer in software trigger mode and send the converted data
to the console |
| Clock Configuration | This
example application shows how to configure the clock system to run
the device at maximum frequency. It also outputs a prescaled clock
signal on a GPIO pin for measurement and verification |
| CRCCU Compute CRC32 | This
example demonstrates how to use the CRCCU module to calculate 32 bit
CRC value of a data block |
| EFC Read Write | This
example shows how to use EFC to erase and program the internal Flash
memory |
| FLEXCOM SPI Blocking | This
example application demonstrates how to use the FLEXCOM SPI
peripheral to transmit and receive a block of data in a blocking
manner |
| FLEXCOM SPI EEPROM Read Write | This
example application shows how to use the FLEXCOM module in SPI
mode |
| FLEXCOM SPI Interrupt | This
example application shows how to use FLEXCOM SPI PLIB with external
loop back to write and then read back an array of data in interrupt
mode |
| FLEXCOM SPI Host Read Write Test
Application | This is a
FLEXCOM SPI Host test application which is provided to demonstrate
communication between SPI host and the corresponding SPI client
application available under -
apps/flexcom/spi/slave/flexcom_spi_write_read/firmware |
| FLEXCOM SPI Client Read Write | This
example application demonstrates how to use the FLEXCOM SPI
peripheral in client mode |
| FLEXCOM SPI with DMA | This
example application shows how to use FLEXCOM SPI PLIB with external
loop back to write and then read back an array of data in DMA
mode |
| FLEXCOM TWI (I2C) EEPROM | This
example application shows how to use the FLEXCOM module in TWI
mode |
| FLEXCOM TWI EEPROM Emulation | This
example application demonstrates how to use the FLEXCOM TWI
peripheral in client mode |
| FLEXCOM USART Blocking | This
example application shows how to use the FLEXCOM module in USART
mode |
| FLEXCOM USART Interrupt | This
example application shows how to use the FLEXCOM module in USART
mode |
| FLEXCOM USART Ring Buffer | This
example application demonstrates how to use the FLEXCOM peripheral
in USART ring buffer mode |
| FLEXCOM USART with DMA | This
example application shows how to use the FLEXCOM module in USART DMA
mode |
| MEM2MEM Memory Transfer | This
application demonstrates data transfer between two memory location
using MEM2MEM |
| PIO Interrupt | This
example shows how to generate GPIO interrupt on switch press and
release, and indicate the switch status using the LED |
| PIO Polling | This
example shows how to poll the switch input, and indicate the switch
status using the LED |
| RSTC Interrupt | This
example shows how to use the RSTC peripheral to generate an
interrupt instead of generating a reset, when the Reset switch is
pressed on board |
| RTC Alarm Interrupt | This
example shows how to use the RTC to configure the time and generate
the alarm |
| RTT Periodic Interrupt | This
example shows how to use the RTT to generate periodic
interrupts |
| SUPC Wakeup Using RTC | This
example shows how to enter different low power modes and exit it
using the RTC alarm |
| SUPC Wakeup Using RTT | This
example shows how to enter different low power modes and exit it
using the RTT alarm |
| SUPC Wakeup Using WKUP Pin | his example
shows how to enter different low power modes and exit it using WKUP
pin |
| Systick Periodic Interrupt | This
example shows how to use the SysTick to generate periodic
interrupts |
| TC Capture Mode | This
example shows how to use the TC module in capture mode to measure
duty cycle and frequency of an external input |
| TC Compare Mode | This
example shows how to use the TC module in compare mode to generate
an active low, active high, and toggle output on compare
match |
| TC Timer Mode | This
example shows how to use the TC module in timer mode to generate
periodic interrupt |
| WDT Timeout | This
example shows how to generate a Watchdog timer reset by emulating a
deadlock |