33.2.5 Pinout Description
The following table shows the functionality of the pin used by the UPDI. See the I/O Multiplexing section in the device data sheet for more information about the UPDI physical pin.
Function | Pin Name |
---|---|
UPDI | UPDI / PF7 |
The following table shows the functionality of the pin used by the UPDI. See the I/O Multiplexing section in the device data sheet for more information about the UPDI physical pin.
Function | Pin Name |
---|---|
UPDI | UPDI / PF7 |