1.2.1 Arduino Compatability
The AVR-IoT Cellular Mini has complete Arduino support through a library built on the top of the open-source DxCore.
To get started with development in the Arduino IDE, follow the steps at iot.microchip.com to install all the required dependencies.
Tip: When the required dependencies are installed,
development for the AVR-IoT Cellular Mini board is also supported in Visual Studio
Code with the extension for Arduino.