1.1.7 PIC32WM BZ6 Curiosity Evaluation Board: Building and Running the SPI Bootloader applications
Path of the application within the repository is apps/spi_bootloader/
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
| Project Name | Description |
|---|---|
| bootloader/firmware/pic32wm_bz6_curiosity.X | MPLABX Project for PIC32WM BZ6 Curiosity Evaluation Board |
Test Application
| Project Name | Description |
|---|---|
| test_app/firmware/pic32wm_bz6_curiosity.X | MPLABX Project for PIC32WM BZ6 Curiosity Evaluation Board |
Setting up PIC32WM BZ6 Curiosity Evaluation Board
SAME54 Xplained Pro Evaluation Kit is used for Host Development kit
PIC32WM BZ6 Curiosity Evaluation Board is used for Target Development kit

- Connect the MOSI Pin 16 (PC04) on EXT2 of the Host development kit to the MOSI Pin on MikroBus 1 of the Target development kit
- Connect the MISO Pin 17 (PC07) on EXT2 of the Host development kit to the MISO Pin on MikroBus 1 of the Target development kit
- Connect the CS Pin 15 (PC06) on EXT2 of the Host development kit to the CS Pin on MikroBus 1 of the Target development kit
- Connect the SCK Pin 18 (PC05) on EXT2 of the Host development kit to the SCK Pin on MikroBus 1 of the Target development kit
- Connect the BUSY Pin 09 (PD00) on EXT2 of the Host development kit to the RST Pin on MikroBus 1 of the Target development kit
- Connect a ground wire between Host development kit and Target development kit
- Connect the Debug USB port on the Host development kit to the computer using a micro USB cable
- Connect the Debug USB port on the Target development kit to the computer using a micro USB cable
Building and Configuring SPI Host Applications
Using SPI SDCARD Host application to send the application binary to Target development kit

If the SDCARD Host Development Kit being used is SAM E54 Xplained Pro Evaluation Kit then follow the steps mentioned in Configuring SDCARD Host application project
Open the SDCARD host application project host_app_sdcard/firmware/sam_e54_xpro.X in the IDE
- If a SDCARD host application project of different development kit is used then open that project in the IDE
Build and program the SDCARD host application using the IDE on to the SPI host dvelopment kit
Open the test application project test_app/firmware/pic32wm_bz6_curiosity.X in the IDE
Build the project to generate the binary (Do not program the binary)
Copy the application binary into the SD card and insert the SD card in the SD card slot available on the SAM E54 Xplained Pro Evaluation Kit
Open the Terminal application (Ex.:Tera Term) on the computer
Configure the serial port settings for Host Development kit as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Jump to Running The Application
Running the Application
Open the bootloader project bootloader/firmware/pic32wm_bz6_curiosity.X in the IDE
Build and program the application using the IDE on to the Target development kit
If the test application is being programmed, Open the Terminal application (Ex.:Tera Term) on the computer and configure the serial port settings for Target Development kit as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Press the Switch SW0 on the Host development kit to trigger programming of the application binary
Once the programming is complete,
LED0 on the Host development kit will be turned on indicating success
The target development kit need to be reset. Press the NMCLR switch, the boot-loader will jump to the user application
If the test application is programmed then RGB_LED_RED should start blinking and you should see below output on the Target development kit console

Press and hold the Switch USR_BTN_1 to trigger Bootloader from test application and you should see below output and then press NMCLR button

Press Reset button on the Host development kit to reprogram the application binary
Repeat Steps 4-5 once
- This step is to verify that bootloader is running after triggering bootloader from test application in Step 6
Additional Steps (Optional)
Using SDCARD Host application
If multiple Target development kit are to be programmed using the same Host development kit then refer to Configuring SDCARD Host application project
Once done repeat the applicable steps mentioned in Running The Application