1.3.1 Bootloader and Application Binary Merge Script Help
This document describes the usage of btl_app_merge_bin.py host script.
Path of the tool in bootloader repository is tools/btl_app_merge_bin.py.
Setting up the Host PC
- The Script is compatible with Python 3.x and higher
Description
-
This script should be used to merge the bootloader binary and application binary
-
It creates a merged binary output where bootloader is placed from start and the application will be placed at the offset passed as parameter
-
If the application offset is not equal to end of bootloader offset it fills the gap with 0xFF until the application offset
-
The merged binary can be used by I2C NVM Host Application as input for Updating bootloader and application together
-
The merged binary will be created in the directory from where the script was called
Usage Examples
Below is the syntax to show help menu for the script.
python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py --help
Below is the syntax and an example on how to merge a bootloader binary and application binary:
python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o <Offset> -b <Bootloader_binary_path> -a <Application_binary_path>
python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o 0x2000 -b <harmony3_path>/bootloader_apps_i2c/apps/i2c_fail_safe_bootloader/bootloader/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin -a <harmony3_path>/bootloader_apps_i2c/apps/i2c_fail_safe_bootloader/test_app/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin