1.5 Offset Error
The offset error is defined as the deviation of the actual ADC’s transfer function from the ideal straight line at zero input voltage.
When the transition from output value 0 to 1 does not occur at an input value of ½ LSB, then we say that there is an offset error. With positive offset errors, the output value is larger than 0 when the input voltage approaches ½ LSB from below. With negative offset errors, the input value is larger than ½ LSB when the first output value transition occurs. In other words, if the actual transfer function lies below the ideal line, there is a negative offset and vice versa. Negative and positive offsets are shown in Figure below.
Since single-ended conversion gives positive results only, the offset measurement procedures are different when using single-ended and differential channels.