1.5.1 How the G3 RF PAL Module Works

Description

The G3 RF Platform Abstraction Layer (PAL) module is the access point to the IEEE 802.15.4 RF PHY layer.

Figure 1-29. RF Platform Abstraction Layer

The G3 RF PAL module offers the necessary functions to control the RF IEEE 802.15.4 PHY layer, which include:

  • Module initialization
  • Transmitting and receiving frames
  • Accessing Parameter Information Base (PIB) to get/set configuration parameters
  • Resetting the RF transceiver

Module Initialization

The RF PAL is not initialized at System level (SYS_Initialize).

The first step that a client (RF MAC) has to take when using RF PAL is to initialize it, by calling PAL_RF_Initialize, which takes a pointer to initialization data as parameter (this initialization data includes all the callback functions to receive events from RF PAL; see PAL_RF_INIT for details). This will return a SYS_MODULE_OBJ, which is used to check the status of RF PAL, by calling PAL_RF_Status. The status is checked in each call to MAC_RF_Tasks until PAL_RF_STATUS_READY is returned.

Once the RF PAL is ready, the handle (PAL_RF_HANDLE) is obtained by calling PAL_RF_HandleGet and it will be used to call other functions of the RF PAL module.

Transmitting and Receiving Frames

Frames are sent to the G3 Network using the PAL_RF_TxRequest primitive. The result of the requested transmission is provided by RF PAL by invoking PAL_RF_TxConfirm callback.

Received frames are reported by RF PAL by invoking PAL_RF_DataIndication callback.

Accessing Parameter Information Base (PIB)

Parameter Information Base (PIB) is a set of parameters that can be accessed for reading and/or writing. They serve mainly 2 purposes: RF PHY layer configuration through PIB writing and information retrieval through PIB reading.

The reading and writing of parameters are made by means of PAL_RF_GetRfPhyPib and PAL_RF_SetRfPhyPib primitives, respectively.

A list of available parameters is found on PAL_RF_PIB_ATTRIBUTE definition.