4 Run the Application
The Linux image prepared in the previous section is an application which is acting as a Wi-Fi station client to connect to the default AP (SSID: DEMO_AP, Password: password). The Light Emitting Diode (LED) on the host Memory Protection Unit (MPU) evaluation board blink in blue when it is connecting to the network and turn on in blue color when it success to connect to the network. The SSH and mDNS feature is enable so that user can remote login to the platform with the platform’s host name for evaluation. User’s can also access the console of the evaluation board for further evaluation.