23.3.3.1.1 Clock Operation
The XCK pin direction controls whether the transmission clock is an input (Client mode) or an output (Host mode). The corresponding port pin direction must be set to output for Host mode or input for Client mode (PORTx.DIRn). The data input (on RXD) is sampled at the XCK clock edge, which is opposite the edge where data are transmitted (on TXD), as shown in the figure below.
The I/O pin can be inverted by writing a
            ‘1’ to the Inverted I/O Enable (INVEN) bit in the Pin n Control
         register of the port peripheral (PORTx.PINnCTRL). When using the inverted I/O setting for
         the corresponding XCK port pin, the XCK clock edges used for sampling RxD and transmitting
         on TxD can be selected. If the inverted I/O is disabled (INVEN = 0), the
         rising XCK clock edge represents the start of a new data bit, and the received data will be
         sampled at the falling XCK clock edge. If inverted I/O is enabled (INVEN =
            1), the falling XCK clock edge represents the start of a new data bit,
         and the received data will be sampled at the rising XCK clock edge.