1.5 I2C EEPROM Read Write
This example application demonstrates how to use the I2C peripheral to write and read from the I2C serial EEPROM memory.
Description
This example uses the I2C peripheral library to write an array of values to the I2C Serial EEPROM and verify the value written by reading the values back and comparing it to the value written.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/i2c/master/i2c_eeprom/firmware .
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| cec1736_evb.X | MPLABX project for CEC 1736 Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board |
|---|---|
| cec1736_evb.X | CEC 1736 Development Board |
Setting Up CEC 1736 Development Board
- Interface the EEPROM 3 click Board by making the
following connections:
- Connect a wire from GPIO140 (I2C06_SCL) available on Pin 28 of P4 header to the SCL pin of the EEPROM 3 click board
- Connect a wire from GPIO132 (I2C06_SDA) available on Pin 26 of P4 header to the SDA pin of the EEPROM 3 click board
- Connect GND and VCC between the EEPROM 3 click Board and the CEC 1736 Development Board
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and Program the application using its IDE
- LED indicates success or failure:
- The LED is turned ON when the value read from the EEPROM matched with the written value
- The LED is turned OFF when the value read from the EEPROM did not match with the written value
The following table provides the LED name:
| Board | LED Name |
|---|---|
| CEC 1736 Development Board | LED5 |