3 Interpreting the Measurement Plots
Markings in the following figure explain how the measurement plots must be interpreted and which values have to be observed across the application note. From the following figure, it is observed that the first plot is always interpreted as the current profile, the second plot as GPIO and the third plot as Reset.