6.4.2 The Keyboard Task
The keyboard task tsk_keyboard() is the task that handles the
button pushes. If the state of one of the buttons is changed, the new state is put into
the key_queue. The receiver of the key_queue is the
main task which is described in the next section. Refer to the figure below for the UML
diagram.