4.4 Get Device Support for MPLAB® X
MPLAB X: Support for new devices in MPLAB X can be added by using the MPLAB Pack Manager, which is found under Tools → Packs.
For the AVR® DD Family, update to the latest version by
performing the following steps:
- Click Check for Updates.
- For the AVR® DD Family, select the latest available version of AVR-Dx_DFP.
- Click Install.
For offline installers, go to packs.download.microchip.com/. To install a package, double click on the installer file and follow the instructions. Any open MPLAB X window will have to be closed for the installation to take effect.