4.2 Get Code Examples from GitHub
The code examples are available through GitHub, a web-based server that provides the
application codes through a Graphical User Interface (GUI). The code examples can be
opened in both Microchip Studio and MPLAB X. To open the Microchip Studio project in
MPLAB X, select from the menu File → Import → Microchip Studio
Project and navigate to the .cproj file.
The GitHub webpage: GitHub.
Code Examples
Finding code examples for devices in the AVR DD Family can be done by searching for the device name, e.g., AVR64DD32, in the GitHub example browser.
Download the code as a .zip file from the example page on
GitHub by clicking the Clone or download button.