3.5 USB HID Host Mouse Driver Library

Topics

Name Description
Introduction Introduces the MPLAB Harmony USB HID Host Mouse Driver Library.
Using the LibraryThis topic describes the basic architecture of the USB HID Host Mouse Driver Library and provides information and examples on its use.
Configuring the LibraryDescribes how to configure the USB HID Host Mouse Driver.
Library InterfaceThis section describes the Application Programming Interface (API) functions of the USB HID Host Mouse Driver Library.The USB Mouse driver does not require explicit API call by the application to obtain Mouse data. The data in the appropriate format is sent to the application during an application event handler function call.
FilesThis section lists the source and header files used by the library.