Name | Description |
Introduction | Introduces the MPLAB Harmony USB Mass Storage Device (MSD) Host Client Driver
Library. |
Using the
Library
| This topic describes the basic architecture of the USB MSD Host Client Drier
Library and provides information and examples on its use. |
Configuring the Library | Describes how to configure the USB Host Layer. |
Library
Interface | This section describes the Application Programming Interface (API) functions
of the USB MSD Host Client Driver Library. Refer to each section for a detailed
description. |
Files | This section lists the source and header files used by the library. |