2.8 USB MSD Device Library

Topics

Name Description
IntroductionIntroduces the MPLAB Harmony USB Mass Storage Device (MSD) Library.
Using the Library This topic describes the basic architecture of the USB MSD Device Library and provides information and examples on its use.
Configuring the LibraryDescribes how to configure the MSD Function Driver.
Library InterfaceThis section describes the Application Programming Interface (API) functions of the USB MSD Device Library.Refer to each section for a detailed description.
FilesThis section lists the source and header files used by the library.