2.8.3 Configuring the Library

The following configuration parameters must be defined while using the MSD Function Driver. The configuration macros that implement these parameters must be located in the system_config.h file in the application project and a compiler include path (to point to the folder that contains this file) should be specified.

Macros

Name Description
USB_DEVICE_MSD_INSTANCES_NUMBERNumber of MSD function Driver instances required in the USB Device.
USB_DEVICE_MSD_LUNS_NUMBER Defines the number of LUNs per MSD function driver instance.
Configuration on MCCThis section describes the symbols available in the MCC that can be configured.